Controlled by Liquiline Control
Automated nitrogen removal in Stadtlohn wastewater treatment plant
The Stadtlohn WWTP regulates nitrogen reduction using the Liquiline Control. The control system regulates the air supply into the aeration basins depending on the current concentration of nutrients in the wastewater.
The results
-
Safe compliance with limit values.
Stable operation.
Optimized energy usage.
High level of process transparency combined with ease of use.
The switching of the basins from parallel to cascade operation during a plant upgrade posed no problem for the control system.
The challenge
The customer required a control system that automated nitrogen reduction while also ensuring compliance with the official nitrogen value in the plant outlet (TN ≤ 8 or 12 mg/l, depending on the time of year). It was also important that the control system would be able to function after the clarifiers were switched from parallel to sequential operation. The upstream basin is now used at the peak-load stage, while the second basin is subsequently used at the low-load stage.
The nitrogen concentration in the outlet had to be as constant as possible during both peak- and low-load phases. Furthermore, the solution had to be easy to operate, to ensure that staff could make settings quickly and easily when on standby duty during the night and at weekends.
Our solution
The WWTP operator opted for a complete solution comprised of several different components:
One oxygen sensor per basin as well as an ion-selective sensor for ammonium and nitrate.
Programmable logic controller (PLC) with Liquiline Control software, which controls both basins individually.
Touchscreen display used to operate the system from the control room.
Various services, such as consulting, design and configuration of the controller, process integration, system training.
Load-dependent aeration control in Stadtlohn
The customer wanted the two aeration basins in the plant to be aerated individually. Sensors in both basins measure the parameters ammonium, nitrate and oxygen. Using the measured values, the Liquiline Control control system configures a dynamic set point for oxygen: depending on the ammonium concentration, the exact amount of air required for complete removal of the ammonium (NH4-N) is injected. This results in process stability while also optimizing the energy efficiency of the blowers.
In addition, the controller dynamically adjusts the duration of the nitrification and denitrification phases. This improves the reduction of total nitrogen (TN), ensuring that it remains at a constant level in the plant outlet.
Remote access to Liquiline Control control system
For the Stadtlohn WWTP, the controller was fitted with a remote control unit. This means that staff on standby duty are able to monitor the process and intervene if necessary from the comfort of their own homes.
FLEX 선택 | 기술적 우수성 | 단순성 |
---|---|---|
Fundamental 선택 기본적인 측정 요구사항 충족 |
기술적 우수성
|
단순성
|
Lean 선택 핵심 프로세스를 손쉽게 처리 |
기술적 우수성
|
단순성
|
Extended 선택 혁신적인 기술로 프로세스 최적화 |
기술적 우수성
|
단순성
|
Xpert 선택 가장 까다로운 어플리케이션 요구사항 충족 |
기술적 우수성
|
단순성
구성에 따라 다름 |